The hidden champions
Novanta is dedicated to making a positive impact on the lives of people around the world. The drive to advance surgical operative technology to improve patient outcomes whilst reducing healthcare costs requires innovative solutions. With over 40 years of experience, we’ve established ourselves as a trusted developer and preferred provider of critical ‘under the hood’ OEM solutions for surgical operative equipment. Leveraging this heritage, we’ve established deep expertise across a series of vital core technologies including insufflators, pumps, endoscopic camera technologies and RFID tracking, all of which play integral roles in operating rooms worldwide. Our unwavering commitment to developing and delivering such crucial solutions contributes to enhancing the current standards of care in surgical settings globally.

Minimally Invasive Surgery
In the realm of Minimally Invasive Surgery, visibility and small, precise incisions are essential. Insufflators and pumps are key enabling technologies in this area.
For over 30 years, Novanta has been a global leader in surgical insufflator technology for laparoscopy applications and surgical pump systems in gynecology. As a pure OEM developer in this area, Novanta is your complete end-to-end system integration partner, who fully understands how to seamlessly interface our pump capability into your technology stack interfacing and firmware requirements that come from embedding our technology into a mission-critical system. Learn more about the OEM surgical technology that we develop that our impact on patients worldwide

Medical Robotics
The medical robotics revolution is well in effect, and surgical robotics platforms are being widely adopted due to the complementary advantages to minimally invasive procedures. Novanta manufactures a series of technologies that are integrated deeply into the surgical robotic systems. These include customizable servo drives, force torque sensors, and unique machine vision camera technology, which together deliver the requisite precision, compactness, reliability, and customization flexibility that has led to us being regarded as a market leader in the field of motor and control technology for these incredible mission-critical applications.

Ophthalmology & OCT
Optical Coherence Tomography, commonly known as OCT, is a noninvasive imaging test that allows eye care professionals to take detailed, cross-sectional pictures of the retina — the part of the eye responsible for vision. Using scanned laser light, OCT captures micrometer-resolution, three-dimensional images from within the retina which in turn help in diagnosing and managing various eye conditions such as glaucoma, macular degeneration, and diabetic eye disease.
Novanta has a long association with ophthalmic applications, and provides a series of camera and scanning technologies to a number of the processes that are used in this field, including Scanning Laser Ophthalmoscopy (SLO) and active techniques such as Laser Assisted In-situ Keratomileusis (LASIK)