Search icon

Search (start typing to perform searching)

Novanta Announces Financial Results for the Fourth Quarter and Full Year 2025

At the heart of the system.

Mission critical products and embedded technologies for next generation medical and diagnostic applications.

Surgical Robotics

The surgical robotics market is advancing at an unprecedented rate. Robot-assisted surgery offers significant benefits across many surgical fields, gaining recognition from hospitals and prospective patients. This trend drives the growth of the sector and the advancement of technologies used in surgical robotics. Although often unseen by the public, robot motion control components play a crucial role in ensuring safe, precise, and efficient robotic procedures. Novanta is enabling the advancement of this incredible technology through several of its precision motion and force torque sensing product lines and technology streams.

Haptic Systems

Haptic feedback technology is crucial to surgical robotics. This technology enhances the surgeon’s ability to perform complex procedures with increased precision and safety by simulating the sense of touch through robotic instruments, and thus providing real-time tactile feedback to the surgeon. Not only does this enhance precision and safety during delicate procedures, it also has the potential to improve patient outcomes and reduce surgical complications. Novanta is a leader in the core haptic engines that live at the heart of these systems, based on our unique miniaturized servo driver, and encoder technologies.

Minimally Invasive Surgery

In Minimally Invasive Surgery, high visibility and precise incisions are critical. However, both are only possible when there is sufficient internal space created to accommodate endoscope and medical instruments. Novanta is a global leader and pioneer of the insufflation, pump, and consumable technologies that are used to perform these critical pumping and insufflation procedures in the field of laparoscopy and gynecology.

Multiomics & Sequencing

Multiomics and DNA sequencing are amongst several exploding biotechnologies that are driving the rapidly expanding personalized medicine industry. Since the 1970s, the time to sequence the human genome has become exponentially faster, through the use of unique lasers and beam shaping technology. Novanta is a leader in developing dedicated laser and positioning engines that are embedded into the instruments that perform these tasks, delivering a unique and precise combination of wavelength, power, reliability required by such instruments.

OCT & Ophthalmology

Optical Coherence Tomography, or ‘OCT’, is a non-invasive imaging procedure that enables eye care professionals to capture detailed, cross-sectional pictures of the retina – the part of the eye responsible for vision. Using scanned laser light, OCT captures micron resolution, 3D images from the retina, which in turn helps diagnose and manage various eye conditions such as glaucoma, macular degeneration, and diabetic eye disease. Novanta has a long association with ophthalmic system applications, and provides customizable imaging sensors and laser scanning technologies to many of the processes that are used in this field, including Scanning Laser Ophthalmoscopy (SLO) and active techniques such as Laser Assisted In-situ Keratomileusis (LASIK).

Microscopy

In recent times, the microscopy industry has witnessed a significant evolution, driven by AI and other technological advancements that together have expanded the frontiers of cellular biology, material science, and automated microscopy. Novanta has established deep heritage in these applications from multi wavelength, fiber coupled laser engines and galvanometer scanners for cellular fluorescence applications, across to custom image sensor technologies together designed to fluoresce, scan, and image cellular structures with ultimate precision.  

Lab Automation

Lab Automation is fast becoming a strategic priority for R&D labs. The close integration of robotics and automated sample handling has significantly shortened cycle times and increased throughput. A key enabler of this revolution is Novanta’s proprietary Radio Frequency Identification (RFID) technology which has revolutionized lab workflows by enabling the tracking and monitoring of samples and equipment with unprecedented precision and efficiency. Our RFID technology streamlines operations whilst enhancing safety by reducing human error and ensuring the integrity of samples throughout the transportation and handling process – crucial factors within drug discovery and diagnostics applications.

  • Allegro IVD Programmable Smart Camera

    Preconfigured for specific In-vitro imaging applications thanks to our embedded Clarity™ 3.0 Machine Vision Software

  • 83 Series Galvanometers

    The industry standard. Always fast, always reliable, and available with a huge range of mirror and coating options.

  • New
    Axia Force Torque Sensors

    Axia Force Torque Sensors

    Expanded series of easy-to-use Force/Torque Sensors supporting a broad range of applications.

  • CRS Resonant Scanner

    Ultra fast realtime scanning up to 12 Khz in a compact package. The mainstay of ophthalmic and other ultrafast scanning…

  • Denali Drive

    Denali

    The smallest servo drive in the market.

  • Everest S NET

    Everest S

    The most power-dense servo drive on the market.

  • FM 8 Configurable Barcode Scanner

    Our fully customizable image based 1D/2D barcode scanners with optional machine vision capabilities.

  • Polygon Ultrafast Laser Scanner

    The pinnacle of ultra high speed laser beam scanning. Up to 55k RPM with extreme durability thanks to our patented…

  • New

    ThingMagic M7e UHF RAIN®

    The latest version of our ThingMagic RFID module combining low power consumption in a tiny form factor!

  • New
    Denali Safe NET

    Denali Safe

    The smallest, most power-dense servo drive ever, now available with Certified Functional Safety.

  • Aura Optical Encoder

    Aura

    Our latest, most advanced optical encoder technology in the smallest footprint available.