JADAK launches entire series of ThingMagic® M7e modules

Press Release

JADAK launches entire series of ThingMagic® M7e modules

Published on May 11, 2024

The smallest UHF RFID modules on the market with the lowest power output. Syracuse, N.Y. (May 11, 2023) – JADAK, a business unit of Novanta Corporation (“Novanta”), announces the release of the ThingMagic® M7e Series featuring the new Impinj E family RAIN RFID reader chips. The M7e Series features five modules, and are the smallest…

The smallest UHF RFID modules on the market with the lowest power output.

Syracuse, N.Y. (May 11, 2023) – JADAK, a business unit of Novanta Corporation (“Novanta”), announces the release of the ThingMagic® M7e Series featuring the new Impinj E family RAIN RFID reader chips. The M7e Series features five modules, and are the smallest UHF RFID modules on the market, enabling customers to use the chip in extremely small applications such as handheld RFID scanners, wearable RFID devices, surgical hand scanners, mobile RFID printers and smart vending machines. JADAK will work with healthcare OEMs, retailers, and CPG customers to integrate the module into unique applications worldwide.

“The new ThingMagic® M7e Series is a natural fit for critical use cases and will further unlock new IoT device opportunities,” said Matt Branda, Impinj vice president of product management. “The small size and low power consumption of the Impinj E family reader chips allow manufacturers to easily add RAIN RFID functionality to devices, and we’re thrilled to enable industry-leading outcomes for JADAK’s customers around the globe.”

In addition to the small size, the modules boast ultra-low power consumption, a necessary requirement for mobile RFID printers, handheld or battery-operated devices used in the retail and inventory tracking spaces. And, each module is capable of varying read rates to accommodate a wide variety of application needs.

One of the most unique features of the M7e Series, as well as all other ThingMagic® modules from JADAK is obtaining certification for select countries in advance. JADAK has extensive expertise in regulatory certification and works to obtain these certifications prior to launch, easing the burden on OEMs to obtain their own regulatory certification.

Additional benefits to customers include accuracy, speed, and the ability to track consumer behaviors over time, allowing for inventory changes to better match customer expectations. And the entire M7e Series is also supported by ThingMagic® Mercury API, a standardized API used across all ThingMagic® products.

“We worked closely with Impinj, a leader in the industry, to develop these high-performance RAIN RFID modules,” said Harinath Reddy, Sr. R&D Director, RFID, JADAK. “These new modules are optimized to achieve the highest read/write and thermal performance while consuming low DC power, which is very critical for our supply chain logistics, retail, and healthcare customers. In addition, some of the M7e modules are drop-in compatible with our M6e modules, allowing our customers to easily migrate to the new modules.”

For more product information, visit https://www.jadaktech.com/product/thingmagicm7e-uhf-rain-rfid-module-series/


About JADAK

JADAK, a business unit of Novanta, is a market leader in machine vision, RFID, barcode, printing, and color and light measurement products and services for original equipment manufacturers. The business designs and manufactures automated identification and data collection solutions that help customers solve unique inspection, tracking, scanning and documenting challenges. JADAK is based in Syracuse, New York, with sales and technical locations across the globe. For more information, visit www.jadaktech.com.

About Novanta

Novanta is a trusted technology partner to OEMs in the medical and advanced industrial technology markets, with deep proprietary expertise in photonics, vision, and precision motion technologies. For more information, visit www.novanta.com.

Upcoming events

Stay informed about our latest events! Join us for exclusive insights, networking opportunities, and the unveiling of our newest innovations. Don’t miss out on the chance to connect with industry leaders and explore cutting-edge advancements.

Subscribe to our Email Newsletter

For subscription management

Name(Required)
Address(Required)