Sept 14, 2026
Novanta Unveils New 3-Axis Integrator Package at IMTS 2026 – Read the Press Release

Article

Superresolution Microscopy Reaches 14 nm

Technical Paper Overview

Choosing the Right Laser Source for 14 nm GSD Super-Resolution
Donut-zero contrast, not laser wattage, decides GSD’s resolution floor.

The Abbe criterion stops conventional confocal microscopes at roughly half the excitation wavelength — fine for cells, useless for finding paired NV-centres in diamond a few nanometers apart. Ground State Depletion (GSD) breaks through it by saturating fluorescence with a donut-profile beam. But the achievable resolution scales with how dark the donut minimum actually is. A laser that can’t hold its TEM₀₀ mode purity, or whose pointing drifts under increased power, produces a donut bottom that isn’t truly dark — and the resolution-versus-power curve flattens out before it should.

This technical paper documents a GSD optical layout at Professor Fedor Jelezko’s University of Ulm group resolving NV-centres to 14 nm FWHM — achieved by scaling the Novanta Laser Quantum gem 532 nm excitation through 8.3, 17.3, 38, and 85 mW while preserving beam purity and pointing stability across the full power range, with the resolution-vs-power curve fitted to the GSD saturation model.

Key takeaways include:

  • Why donut beam quality — not raw laser power — sets the ultimate resolution floor: a non-zero donut minimum caps resolution before saturation does
  • How NV-centre fluorescence saturation flips diffraction-limited imaging into power-scalable super-resolution — and what laser-source specs survive the scaling
  • When to specify a stabilized gem 532 over generic 532 nm sources: applications where the same laser must hit 8 mW and 85 mW while holding beam pointing and mode purity
  • What the gem 532 brings to GSD: TEM₀₀ mode purity, low pointing drift across the full power range, and the long-term stability that makes the resolution-vs-power calibration trustworthy
  • A practical forward-looking note: NV-centre super-resolution sits at the intersection of quantum information processing (coupled qubits) and biology (proteins on nano-diamonds) — two growth markets the same laser serves

Download the full technical paper for the GSD optical layout diagram from the University of Ulm group, the four-power image series showing the dark-spot collapse from confocal-limited to 14 nm, and the resolution-versus-power fit — before specifying a 532 nm source on average-power spec alone and discovering at 85 mW that beam quality, not laser power, is what’s capping your resolution.

Newsletter Sign-up

This field is for validation purposes and should be left unchanged.

Gated Content

This field is for validation purposes and should be left unchanged.
This field is hidden when viewing the form