Sept 14, 2026
Novanta Unveils New 3-Axis Integrator Package at IMTS 2026 – Read the Press Release

Article

Semiconductor Electronics Inspection

Technical Paper Overview 

Wafer Surface Analysis: Detecting Defects With Laser Solutions Catching a wafer defect early depends on a laser that holds steady power and beam quality 24/7.

Semiconductor wafers are inspected for surface defects at every stage of manufacturing, and at least three times: when the wafer is created, at incoming quality control at the chip plant, and during and after development of the microchips. Any surface defect renders a chip unusable, so many of these inspections use lasers for their measurement precision and resolution. Laser light is rapidly scanned across the wafer’s surface or edge with a high-speed polygon scanner, and any deviation in the reflected light indicates a defect.

This white paper covers what that demands of the laser: long lifetime, maintenance-free operation, passive water-free cooling, controlled speckle patterns, exceptional beam quality, zero power fluctuation, and the resolution to image ever-smaller features. It then shows how Laser Quantum’s axiom LE addresses them: a 12 W air-cooled laser that avoids the liquid cooling widely prohibited in this application, with a customized bandwidth profile for the inspection’s speckle pattern, active noise suppression, and integrated power feedback.

Key takeaways include:

  • Why wafers are inspected at least three times, and why one surface defect can make scrapping a wafer early cheaper than running it through the rest of the process
  • How laser wafer inspection works: a high-speed polygon scanner sweeps the beam across the wafer surface or edge, and changes in the reflected light flag defects
  • The seven laser requirements that make deployment hard: long lifetime, maintenance-free operation, passive water-free cooling, controlled speckle, exceptional beam quality, zero power fluctuation, and smaller-feature imaging
  • Why air cooling matters: liquid cooling is widely prohibited in this application, and the axiom LE delivers 12 W without it
  • What a customized bandwidth profile, active noise suppression, and integrated power feedback add: a speckle pattern tuned to inspection and a beam specification that holds with no power fluctuations, plus remote maintenance and service access

Download the full white paper for the complete list of laser requirements, the three-stage wafer inspection process, and a closer look at how the axiom LE’s air-cooled design, customized speckle profile, and integrated power feedback support 24/7 wafer inspection. Then talk to an application engineer about the laser your inspection system needs.

Newsletter Sign-up

This field is for validation purposes and should be left unchanged.

Gated Content

This field is for validation purposes and should be left unchanged.
This field is hidden when viewing the form