Everest S

Celera Motion Introduces World’s Smallest, Fastest Servo Drive

Published on October 20, 2022

The new blisteringly fast Everest S is about 30% smaller, includes Dual-BISS-C feedback support and is ideal for surgical robots, exoskeletons and other applications

BEDFORD, Mass. (Oct. 20, 2022) — Celera Motion, an award-winning business unit of Novanta Inc., today announced the introduction of the world’s smallest and fastest servo drive.

The new Everest S, the latest addition to the popular Everest Series, is about 30% smaller than its predecessor, making it the world’s smallest servo drive. It’s also the fastest: The EtherCAT and CANopen versions deliver bus latency reduced to 1 cycle, making Everest S the fastest servo drive on the market today.

The Everest S includes all the best features of other Everest servo drives — plus it now also includes Dual BiSS-C feedback support, a highly sought-after feature. And because it combines 16-bit differential current and four configurable ranges, Everest S delivers flawless resolution and is ideal for virtually any market application.

“We’re excited to introduce the Everest S to meet the growing demand for smaller, faster servo drives that provide more space for applications and even better performance,” said Marc Vila, Director of Strategy & Business Development for Celera Motion. “Our goal is to give product designers as much freedom and flexibility as possible, and the Everest S delivers that and more.”

Designed with 3 kW of power and a starting weight of just 18 grams, the Everest S is ideal for applications such as surgical robots, exoskeletons, Pan Tilt gimbals, collaborative robots, legged robots, and autonomous mobile robots.

The Everest S offers several advantages, including:

  • Best-in-class motion-control performance, efficiency, and integration capabilities
  • An optimized hardware architecture that allows for high-speed communication protocols with minimum latency
  • A current loop running at 50 kHz and a velocity loop at 25 kHz, guaranteeing optimal performance for motors
  • An ultra-compact design with an extremely low profile and a lightweight design
  • Multiple integration options and superior power management
  • The latest motion-control software with a user-friendly configuration wizard and diagnostics.

High-speed SPI bus communication is available for optimized EtherCAT/CANopen multi-axis architectures. Everest S also has been designed to meet industrial functional safety standards to ensure continuous safe operation.

Everest S is the latest version of Summit Servo Drives Series. Others include the Capitan Series and the Denali Series.

To learn more about the Everest S Series, visit https://www.ingeniamc.com/everest-s-series/.

About Celera Motion

Celera Motion, headquartered in Bedford, Massachusetts, is a market-leading provider of motion-control components and subsystems for OEMs serving a variety of medical and advanced industrial markets. Celera Motion offers precision encoders, motors, and customized mechatronic solutions that help customers solve challenging motion-control problems. For more information, visit www.celeramotion.com

About Novanta

Novanta is a trusted technology partner to OEMs in the medical and advanced industrial technology markets, with deep proprietary expertise in photonics, vision and precision motion technologies. For more information, visit www.novanta.com.

Lorem ipsum dolor sit amet, consectetur adipiscing elit, sed do eiusmod tempor didunt ut labore et dolore magna aliqua. Ut enim ad minim.

Default Image