Sept 14, 2026
Novanta Unveils New 3-Axis Integrator Package at IMTS 2026 – Read the Press Release

Article

Calibration Accuracy for Laser & Scan Head Sub-Systems

Technical Paper Overview

Calibration Accuracy for Laser & Scan Head Sub-Systems Calibration method, not scan head spec, decides Mark-on-the-Fly accuracy.

Calibration accuracy is the spec that quietly decides whether dynamic-positioning laser applications work. For static jobs — repetitive marking at fixed positions — factory pre-settings work. But for Mark-on-the-Fly, camera-based positioning, semiconductor, and e-mobility, the X/Y mirror pincushion plus F-Theta lens barrel distortion compound into positioning errors that no post-process adjustment can correct.

This technical paper from three Novanta authors compares three calibration methods (hand, flatbed scanner, metrology) across two Cambridge Technology scan heads (VERSIA hybrid + Lightning II full digital) on paper and glass substrates — with empirical results: hand calibration delivers ~1% scan-field error, flatbed ~0.1%, and metrology limited only by the MicroVu’s intrinsic precision.

Key takeaways include:

  • Why calibration accuracy gets ignored on spec sheets but decides Mark-on-the-Fly and camera-based positioning success
  • How X/Y mirror pincushion and F-Theta lens barrel distortion compound into the calibration challenge
  • When to invest in metrology calibration (e-mobility, semiconductor) versus hand calibration (factory marking presets)
  • What each method delivers: hand (~1% error, minutes), flatbed (~0.1%, ~1 hour), metrology (lowest error, highest cost)
  • A practical scan-head + substrate matrix: Lightning II + glass = lowest error in metrology calibration

Download the full technical paper for the three-method calibration comparison data (VERSIA vs Lightning II × paper vs glass), the equipment list (IPG fiber laser, Jenoptik F-Theta, MicroVu metrology), and the time/cost/accuracy tradeoff curves you can use to specify the right calibration approach for your application before commissioning the line.

    Newsletter Sign-up

    This field is for validation purposes and should be left unchanged.

    Gated Content

    This field is for validation purposes and should be left unchanged.
    This field is hidden when viewing the form