Sept 14, 2026
Novanta Unveils New 3-Axis Integrator Package at IMTS 2026 – Read the Press Release

Article

The Benefits of Ultrashort Pulses in Two-Photon Microscopy

Technical Paper Overview

Choosing an Ultrashort Pulse Laser System for Two-Photon Microscopy
Pulse duration at the sample, not at the laser output, decides TPM benefit.

Two-photon microscopy has stood still on a 100-150 fs / 80-100 MHz excitation envelope for nearly thirty years — not because sub-10 fs pulses don’t help (they do: deeper imaging, higher fluorescence efficiency, multi-fluorophore excitation without tuning, less photo-damage), but because every additional optic between the laser and the sample stretches the pulse. By the time a sub-10 fs pulse reaches the focal plane through a standard 63× objective, dispersion has destroyed most of what the laser delivered. The result: most life-science labs don’t have a resident photonics engineer to manage chirped-mirror pre-compensation, so they default to safer 150 fs pulses and accept the imaging-depth ceiling.

This technical paper documents how Novanta’s venteon ultra (<5.5 fs measured), venteon vChirp dispersion-modeling software, DCM chirped-mirror set, and d-scan pulse-characterization + auto-compression unit work as a closed-loop system that delivers 6.4 fs FWHM pulses at the sample plane through a standard 63×, 0.75 NA objective — without requiring photonics expertise at the microscope.

Key takeaways include:

  • Why sub-10 fs pulses have remained specialist for 30 years — dispersion through the microscope optical train destroys what the laser delivers
  • How vChirp + d-scan close the loop: software models the beam path, characterization measures the pulse at the sample, auto-compression adjusts in real time
  • When to specify the venteon ultra system over a stock 100 fs Ti:Sapphire: deep-tissue imaging, multi-fluorophore excitation, photo-damage-sensitive live-cell experiments
  • What the venteon ultra delivers: <5 fs transform-limited / <5.5 fs measured pulses, broad spectral output covering the full Ti:Sapphire emission range
  • A practical workflow: input the beam-path optics into vChirp → predict the chirped-mirror stack → measure with d-scan at the sample → auto-compensate

Download the full technical paper for the optical-train schematic with the d-scan auto-compression loop, the dispersion-modeling logic behind vChirp, and the measured 6.4 fs FWHM result after a standard objective — before specifying a 100 fs TPM source and capping your imaging depth, contrast, and multi-fluorophore range on dispersion you could have compensated for.

Newsletter Sign-up

This field is for validation purposes and should be left unchanged.

Gated Content

This field is for validation purposes and should be left unchanged.