Article

What is the Difference? Beam Size vs. Clear Aperture

Published

Reading time

Category

Understanding Laser Beam System Designs:  Beam Size versus Clear Aperture

For system set ups, it is important to understand the design of laser beam systems that utilize beam steering technology.  More specifically, pairing a beam steering set with a laser is crucial.  During set up, aligning the clear aperture of the beam steering set with the beam size of the laser is critical.  This often raises the question between beam size and clear aperture.  Let’s dissect this issue in this blog post, as well as help you with proper calculations.  

Setting Up Laser Beam Systems

There are many misconceptions regarding the set-up of a laser and beam steering system.  The most common misconception is that the clear aperture value should equal the maximum allowable laser beam size.  Optic components have a parameter known as clear aperture, which strictly defines the optical performances within this aperture.  Optics performance outside of the clear aperture are unspecified.  Significant illumination beyond this boundary not only causes power loss, but will also cause the optics to do the following:  

  1. Deformation of the optic due to excessive heating
  2. Change in index of refraction with temperature (transmissive optics only)
  3. Delamination between the coating and the substrate
  4. Stray light which can damage other components of the system

Beam Size versus Clear Aperture: The Gaussian Profile

Typically, lasers emit circular shaped beams with a Gaussian profile. By applying beam shaping technologies, the Gaussian profile can be transformed into a Uniform profile (Top Hat), with the output beam shaped as a square, rectangular, etc. The beam size for a Uniform parameter is straightforward (see figure below). Meanwhile measuring the beam diameter of the Gaussian profile is more subjective and heavily dependent on the methodology being followed. Some of the different criteria used for reporting a Gaussian beam size include; D4σ, 10/90 or 20/80 knife-edge, 1/e2, FWHM, and D86. Where 1/e2 and FWHM (Full-Width at Half-Maximum) are most commonly used. Understanding the laser beam profile and beam size is important.  Indeed, the same laser beam will have a different beam size based on its definition1.   

Different Beam Sizes

What happens when the same clear aperture is applied to different beam sizes? Pretty straightforward as shown in the figure below. If the laser beam overfills the clear aperture, it will clip the outer-ring portion of the laser beam. Which brings us to the next question.  What beam diameter should one apply for a certain clear aperture?   

   By digging a little deeper into the math equations and using a typical Gaussian beam with a beam size defined by 1/eas an example, we can ensure <1% of power loss due to beam clipping. See formulas below:  

    Therefore, the incident beam diameter on the aperture should be:  

 And with the same calculation to ensure <10% of power loss, the clear aperture should be at least 1.07 times bigger than the 1/ebeam size; for <5% power loss, it should be 1.22; and for <0.1% power loss, it should be 1.86.   Important to note is that since a laser beam size value defined by 1/eis roughly 1.7 times the diameter defined by FWHM, calculations for the appropriate beam size and clear aperture ratios can be made out of the above examples.   In this case, we define the beam size under FWHM when using the Gaussian beam as an example. . To ensure <1% of power loss due to beam clipping, the clear aperture should be:  

Importance of Laser Beam Size

Another point to clear up is the typical misconception of having the input laser beam size exactly the same as the clear aperture. Applying the same formula, and assuming the beam size is defined by 1/e2, you are at risk of clipping 13.5% of the power. It’s critical to note that the amount of power falling off the mirrors will not only cause heat up, delaminate, burn coatings and scatter light as previously mentioned, but will also be deposited onto the internal parts within the scan head enclosure or be absorbed by the DFM lens retaining ring (with glue) and DFM lens holder. In either case, this will cause major damage to current systems during integration and is especially important when working with a high-power laser.   Last but not least, the above calculations are assuming perfect alignment. If there are actual alignment errors, one should consider keeping some margins. .

Remember the Differences Between Beam Size versus Clear Aperture

In conclusion, always remember that the definition of the input beam size and the clear aperture size is NOT the same. When this is mistaken, it can cause unexpected power clipping which will negatively affect your system during integration like malfunction or even a system explosion. When users purchase a laser beam steering solution from us, we provide the clear aperture information, whereas the definition of the laser beam size should come with the spec sheet of the laser. In addition, the laser spec sheet might also provide laser alignment specs, such as its laser output position and pointing error. If these aren’t provided, make sure to check with the laser manufacturer to confirm these parameters for best performance purposes. Having tested and successfully integrated different systems across multiple applications, we can guarantee that these recommendations will help clear up confusion and prevent future damages.        


1. Some lasers may have a central irradiance profile that closely matches a Gaussian profile but also contain additional “lobes” of irradiance in the wings. At high power, these lobes can be significant and must be taken into consideration.

Newsletter Sign-up

This field is for validation purposes and should be left unchanged.