Key Takeaways
- At Formnext 2022, Novanta and Dyndrite announced a collaboration to let Dyndrite software generate low-level scanning trajectories directly for Novanta FireFly3D and LIGHTNING II scan heads.
- Many laser powder bed fusion (LPBF) machines, including direct metal laser sintering (DMLS) and selective laser melting (SLM) systems, run their scanners below full capability because of standard trajectory strategies.
- Fixed patterns such as checkerboard hatching simplify qualification but can limit efficiency and material microstructure improvements.
- Direct software-to-scanner control opens finer-resolution trajectories, more flexible scan strategies, and potentially faster build rates.
- FireFly3D supports multi-head machine architectures with up to 100% field overlap and built-in process monitoring.
Two Companies, One Better Metal Printing Machine
FRANKFURT, November 15, 2022, Formnext. Novanta, a supplier of laser photonics, precision motion control, and vision technologies for advanced industrial OEMs, including additive manufacturing applications, and Dyndrite™, provider of a GPU-accelerated computation engine for digital manufacturing hardware and software, announced a collaboration in support of Novanta’s FireFly3D and LIGHTNING™ II laser beam steering solutions.
The companies will collaborate on a proof-of-concept that allows Dyndrite software to directly generate low-level scanning trajectories for Novanta hardware. Users of Dyndrite Additive CAM software gain the ability to generate very fine-resolution scanner trajectories that make full use of the advanced functions and underlying power of the laser scanner.
Why Scan Trajectories Matter in Laser Powder Bed Fusion
In laser powder bed fusion, including direct metal laser sintering (DMLS) and selective laser melting (SLM), a galvanometer scanner steers the laser across each layer of metal powder. The path the beam follows, how fast it moves, and how laser power is modulated along the way determine melt pool behavior, part density, and build time.
Novanta’s high-precision scanning solutions are used in a wide variety of LPBF machines but are often not fully utilized by standard trajectory strategies. These scanners can frequently run at much higher performance levels, and with a wider range of scan strategies, than the open market typically makes available today.
FireFly3D Scan Head Capabilities
Engineered as an enclosed, compact solution for multi-head machine architectures with up to 100% overlap, FireFly3D is designed for serial-production, high-throughput additive manufacturing machines. Built-in features simplify installation and operation, including precise monitoring of the additive manufacturing process and synchronized process and motion data.
“High performance scanners such as Novanta’s Firefly 3D and Lightning™ II are designed with smart technology to predict their own capabilities and limits,” said Simon Matthias, Technical Business Development Manager, Novanta. “This informs the controlling hardware how best they can be driven to allow full use of the scanners’ complete bandwidth. We’ve seen what is possible from a materials and process standpoint with Dyndrite, and knew working with them would unlock the full potential of our scanners.”
Beyond Standardized Scanning Patterns
Parameter and scanning-pattern development is a major undertaking when qualifying new materials and machines. As a result, machine users, developers, and the software that drives them often stay with traditional approaches, relying on standardized patterns such as checkerboard or similar hatch-based strategies. The trade-off is often lower efficiency and missed opportunities to improve material microstructures.
Dyndrite aims to change this model of parameter development by giving engineers far more software power, freedom, and control over the scanner. These controls and algorithms can use the full capability of the underlying hardware to support more efficient, lower-cost machine design and better process interactions, which can lead to improved material properties and faster build rates.
“Dyndrite was formed as we saw that the manufacturing hardware had outpaced the software,” said Harshil Goel, CEO, Dyndrite. “Our work with Novanta is one step closer to reversing this industry stifling trend. We look forward to working with the Novanta team and showcasing the combined power of our solutions.”
Dyndrite provides an Application Development Kit (ADK) for building additive CAM solutions across a variety of AM processes. The company also announced a new Materials and Process Development for LPBF software solution based on this ADK, and aims to keep working with machine hardware providers to offer tighter laser controls in its software portfolio.
About Dyndrite
Dyndrite’s mission is to fundamentally affect how geometry is created, transformed, and transmitted on a computer. Its ADK gives hardware and software companies the power, freedom, and control needed to deliver on the potential of digital manufacturing. Learn more at dyndrite.com.
How Novanta Can Help You Get More From Your LPBF Machine
Product spotlight: FireFly3D 3-axis scan head. FireFly3D is built for laser powder bed fusion machines in serial production. Its enclosed, compact design supports multi-head architectures with up to 100% field overlap, and dedicated process-monitoring ports deliver synchronized process and motion data. At its core is the LIGHTNING II digital architecture, with a 24-bit encoder and scanning accuracy of 10 µm or better.
Complete the system. Pair your laser scan heads with Novanta controllers and software, and learn more in How Laser Additive Manufacturing Is Changing Production or on our additive and advanced manufacturing applications page.
Ready to unlock more performance from your metal printing machine? Talk to a Novanta application engineer or request a quote.