A satcom array

Latest Articles

Positioning Systems for Satellite Communication

Published on April 27, 2021

Satellite communication plays a fundamental role in our interconnected global network. Most operational satellites use positioning systems that make these communications possible. These positioning systems are located in different parts throughout the satellite system. Utilizing reliable positioning allows an immense range of data-driven applications, including budding 5G networks and Internet of Things (IoT) connectivity, to…

Satellite communication plays a fundamental role in our interconnected global network. Most operational satellites use positioning systems that make these communications possible. These positioning systems are located in different parts throughout the satellite system. Utilizing reliable positioning allows an immense range of data-driven applications, including budding 5G networks and Internet of Things (IoT) connectivity, to be possible. More satellites are launched into low earth orbit (LEO), medium earth orbit (MEO), and geostationary orbit (GEO) year-over-year. This, among other trends for satellite communications, generates pressure on designers, including increased production of LEO satellites to reduce signal latency.

Satellite Communications

Commercial satellites orbit at altitudes of 160 – 35,786 km from the earth. This exceptionally wide scale covers all three orbital ranges; LEO, MEO, and GEO. Geostationary, or geosynchronous, satellites are preferred for communications applications as they are positioned above the Van Allen radiation belt, which can prove inhospitable to sensitive electrical components. However, it takes approximately 0.22 seconds for satellites in geosynchronous orbit to relay signals, which creates a perceptible latency.

LEO satellites orbit earth at the closest altitudes, which simultaneously reduces latency and coverage. While it takes only a few GEO satellites to provide worldwide coverage, numerous interconnected LEO systems, using careful telemetric components and ground-level antenna pointing systems (APSs), are required to reach such communication levels. However, LEO networks represent an exciting frontier for low latency 5G broadband with widespread interconnectivity.

One of the primary challenges from a satellite communications design perspective is the need for automated APSs that can track the positions of LEO satellites accurately and fast. This may require a mobile solution for example, such as Satcom-on-the-Move (SOTM) APSs for air, land and sea. However, these systems are exposed to harsh atmosphere conditions including moisture, extreme temperatures, dust and several contaminants, such as oil or sand, which are a pervasive risk.

Positioning Systems for Satellite Communication

If Satcom companies are to take advantage of the new horizon of LEO interconnectivity, they must overcome the above-mentioned challenges – designing powerful and robust systems and solving ground issues, such as motion-induced errors in APSs mounted on marine vessels.

Positioning Systems

Due to the number of satellites being designed for orbits like LEO, APS has become an aggressive market. The ultimate decision when selecting a particular APS will depend mostly on its performance tracking and pointing a particular satellite/constellation.

Most APSs require at least two degrees of freedom (DOF) of motion. These two DOF are mainly the azimuth and elevation axis of a gimbal, performing the mechanical steering of an APS. Some APSs require a three or more DOF, depending on the frequency band and location of the terminal. An antenna dish will normally be mounted on that gimbal, to perform the above-mentioned operations. The precision obtained by the gimbal will directly affect the gain and pointing accuracy of the APS.

There are many parameters that will affect the performance of the APS, controlled by the design at a system level. One of the most important factors that will play a significant role in the overall performance of the APS is the quality and precision of the motion-related components on the mechanical steering system, especially because these are very difficult to change once the design has been completed.

APS Components from Celera Motion

Celera Motion offers a suite of high-accuracy components for reliable positioning in antenna pointing systems. The Ultra Incoder

TM

Series of rotary encoders are non-contact inductive angle encoders designed specifically for use in harsh environments, exceling at precise angle measurements with up to 22-bits resolution. This enables high pointing accuracies for Very Small Aperture Terminals (VSAT) with MIL-standard shock and vibration performance, providing admirable resistance to motion-induced challenges.

These low format encoders are also optimized for reliability under fluctuating temperatures. High EMI-immunity and low radiated emissions allows a strong output signal to be packed closely to other navigation equipment that can normally be sensitive to radiated emissions. This high EMI-immunity can allow a smaller footprint, tight package design – keeping all communication equipment in one location.

Inductive Sensor for Satcom

Indutive Sensor for Satcom

Celera Motion has also provided a range of positioning systems suited for lightweight, energy-efficient systems. Read this application story on satellite communications for details.

Interested in learning more about our Satcom-grade rotary encoders? Our Ultra Incoders are available in Mini (37 – 58 mm OD) and Midi (75 – 300 mm OD) sizes to suit varied end-user configurations. Contact us for more details on integrating our best-in-class rotary encoders for your satellite communications system.

Lorem ipsum dolor sit amet, consectetur adipiscing elit, sed do eiusmod tempor didunt ut labore et dolore magna aliqua. Ut enim ad minim.

Subscribe to our email newsletter

Litora mollis natoque molesus elit augue nequme naeos magortis sodtoque molales nec eratmuos loste.

This field is for validation purposes and should be left unchanged.
Address(Required)