Edge computing architecture illustrated near connected devices

Articles

What Is Edge Computing and How Does It Work?

Published on April 28, 2026

Edge computing brings computational and storage capabilities closer to where data is generated and consumed at “the edge of the network”. This enables faster and more efficient data processing while reducing latency and addressing common challenges. These challenges are posed by the volume, velocity and real-time requirements of data generated by IoT and other applications.…

Edge computing brings computational and storage capabilities closer to where data is generated and consumed at “the edge of the network”. This enables faster and more efficient data processing while reducing latency and addressing common challenges. These challenges are posed by the volume, velocity and real-time requirements of data generated by IoT and other applications.

Edge computing can be useful in many different applications. Smart cities, autonomous vehicles, industrial automation, and healthcare benefit through real-time data processing and low latency. Faster and more efficient data processing with edge computing helps organizations make faster and better decisions, improve operational efficiency and provide better customer experiences.

Edge computing architecture illustrated near connected devices

What Is it?

There is no specific law that states that as networks grow, latency also grows. However, it is generally true that as the number of devices on a network increases, the potential for latency and other performance issues also increases.

This is because as more devices are added to a network, more data needs to be transmitted and the overall traffic on the network increases. This leads to congestion, packet loss and other issues impacting network performance and increased latency.

To address these issues, network administrators often use techniques such as Quality of Service (QoS) to prioritize certain types of traffic over others. They may also deploy edge computing solutions to enable real-time processing of data at the edge of the network. This lessens the need for transmitting data over long distances and reduces latency.

The main challenge that edge computing solves is latency. By bringing computation and storage resources closer to where the data is generated and consumed, edge computing can reduce the time it takes to process data. This allows for real-time processing of data and reduces latency. 

Edge computing is critical for applications that require low latency, such as IoT and autonomous vehicles. By processing data locally, edge computing can also lower the amount of data that needs to be transmitted to a centralized data center or cloud, further shrinking latency and warranting more efficient use of network resources.

How It Works

Edge computing works by bringing computational and storage resources closer to where the data is generated and consumed at the network’s edge. This allows for faster and more efficient processing of data, reducing latency and improving overall performance.

The following are the basic steps involved in the edge computing process:

  1. Data is generated by various sources such as sensors, cameras, smartphones or other IoT devices.
  2. The data is collected and processed by edge devices such as gateways or edge servers that are located close to the data source.
  3. Edge devices perform various tasks such as data filtering, data aggregation and data analysis.
  4. The processed data is sent to a central server or the cloud for further processing or storage.
  5. Depending on the use case, edge devices also act on the processed data in real time, taking actions such as adjusting settings, sending alerts or initiating automated processes.
  6. In some cases, edge devices also communicate with other edge devices to share data or coordinate actions, creating a decentralized network of interconnected devices.

Edge Computing Deployments

There are several different deployment types of edge computing that organizations can consider based on their specific use cases and requirements. Some of the most common deployments of edge computing are:

  • Edge devices: Edge devices such as sensors, cameras and other IoT devices are used to collect and process data locally. This deployment model is ideal for applications that require real-time processing and low latency, such as industrial automation and healthcare.
  • Edge servers: Edge servers are placed at the edge of the network to process data locally. Edge servers can provide more processing power and storage capacity than edge devices. This makes them suitable for applications that require more compute-intensive tasks such as data analytics and video processing.
  • Fog computing: Fog computing is a distributed computing paradigm that extends cloud computing capabilities to the edge of the network. In this deployment model, fog nodes are stationed at the edge of the network to process data locally. This provides a hierarchical architecture that enables more efficient data processing.
  • Mobile edge computing: Mobile edge computing (MEC) brings edge computing capabilities to mobile networks. In this model, edge servers are placed at the base stations of mobile networks, enabling faster and more efficient data processing for mobile applications.
  • Cloudlet computing: Cloudlet computing commissions cloud computing capabilities to the edge of the network. In this model, cloudlets are small data centers located at the network’s edge, providing cloud computing capabilities to nearby devices.

Edge Computing Applications

Edge computing is a versatile technology that can be used in a variety of applications across different industries. Some of the most popular use cases for edge computing are as follows:

  • Internet of Things (IoT): Edge computing is an essential component of many IoT applications. Computational and storage resources are brought closer to where the data is generated and consumed. This equips real-time processing of IoT data, reducing latency and improving the overall efficiency of IoT applications.
  • Autonomous vehicles: Edge computing is critical for autonomous vehicles which require real-time processing of large amounts of data. It delegates real-time data processing and decision-making at the edge of the network, minimizing the need for transmitting data to a centralized data center or cloud.
  • Industrial automation: Edge computing is ideal for advanced industrial engineering, such as predictive maintenance and quality control. By processing data locally, it warrants real-time monitoring and control of industrial processes, improving efficiency and shortening downtime.
  • Smart cities: Edge computing can be used in smart cities to enable real-time processing of data from sensors, cameras, and other IoT devices. This can permit more efficient traffic management, improved public safety and better management of utilities.
  • Healthcare: Edge computing can be used in healthcare engineering, like healthcare identity management and real-time health data analysis. It can validate real-time monitoring and analysis of health data, improving patient outcomes and reducing healthcare costs.

Benefits

Edge computing offers several benefits for organizations that adopt this paradigm. The key benefits of edge computing are as follows:

  • Reduced latency: Edge computing brings computational and storage resources closer to where the data is generated and consumed, reducing the time it takes to process data and reducing latency.
  • Improved performance: Edge computing improves the overall performance of applications by processing data locally, reducing the need for transmitting data to and from a centralized data center or cloud.
  • Enhanced security: Edge computing provides enhanced security by keeping sensitive data at the edge, reducing the risk of data breaches or cyberattacks.
  • Cost savings: Edge computing reduces the cost of data transmission and storage by processing data locally, lowering the need for high bandwidth connectivity and storage capacity.
  • Increased reliability: Edge computing creates more reliable systems by reducing reliance on a single point of failure, such as a centralized data center or cloud.
  • Real-time processing: Edge computing enables real-time processing of data, which is critical for applications that require real-time response, such as IoT, autonomous vehicles, and healthcare.
  • Scalability: Edge computing is highly scalable, allowing for the deployment of additional edge devices as needed to handle increased workloads.

The trend in IoT growth has been significant over the past few years and is expected to continue growing. According to various reports and studies, some of the trends in IoT growth are as follows:

  • Increasing number of connected devices: The number of connected devices has been increasing steadily, with estimates ranging from 30 billion to over 75 billion connected devices by 2025. This growth is driven by the increasing adoption of IoT in various industries, such as healthcare, manufacturing and retail operations.
  • Rapid growth in industrial IoT: Industrial IoT (IIoT) is a subset of IoT that focuses on industrial applications, such as manufacturing, supply chain management and energy. IIoT is expected to grow rapidly, with estimates suggesting that the market could reach $933 billion by 2025.
  • Greater adoption of edge computing: As the number of connected devices grows, there is a greater need for real-time data processing and analysis. 
  • Increased use of AI and machine learning: As the volume of IoT data grows, there is a greater need for advanced analytics and machine learning algorithms to process and make sense of this data. AI and machine learning will play a significant role in IoT growth, permitting more intelligent and automated decision-making.

Challenges

Designing and engineering for edge computing can present several challenges for organizations. The critical challenges of edge computing are as follows:

  • Resource constraints: Edge devices are often limited in terms of processing power, memory, and storage capacity. This makes it challenging to design and engineer applications that can run effectively on these devices.
  • Heterogeneous environments: Edge devices come in various shapes and sizes and can run different operating systems and software. This creates challenges to developing and deploying applications that can run across a wide range of devices.
  • Network connectivity: Edge devices often rely on wireless connectivity, which can be unreliable, slow, and subject to interference. It can be difficult to ensure consistent performance across devices.
  • Data management: Managing data across multiple edge devices is sometimes challenging, particularly as the volume of data increases. Organizations need to develop effective data management strategies that can handle the unique requirements of edge computing.
  • Security: Edge devices can be vulnerable to security threats, particularly as they often run in uncontrolled environments. Organizations must develop effective security strategies that can protect edge devices and the data they process.
  • Integration with existing systems: Integrating edge computing with existing IT systems can be challenging. Particularly, many organizations have legacy systems that were not designed to support edge computing.
  • Scalability: As the number of edge devices and the volume of data increases, organizations need to ensure that their edge computing infrastructure can scale effectively to handle the increased workload.

Case Study: Edge Computing in Action

Growing smart cities are learning to harness next-gen edge camera platforms for their modular hardware and software characteristics. The benefits are seen in critical smart city systems like Smart Traffic Management. This gives city managers and urban developers deep visibility into traffic and its patterns over a wide range. 

Read more below:

Lorem ipsum dolor sit amet, consectetur adipiscing elit, sed do eiusmod tempor didunt ut labore et dolore magna aliqua. Ut enim ad minim.

Contact us

This field is for validation purposes and should be left unchanged.
Full Name(Required)
Address
This field is hidden when viewing the form