Accurate light & color calibration

Light and Color Measurement for Medical Imaging

Accurate light and color calibration is essential to medical imaging quality and patient safety. Novanta Photo Research® SpectraScan® spectroradiometers deliver laboratory‑grade measurement accuracy trusted by medical device manufacturers to validate and calibrate illumination systems .

Medical Devices Require Precise Light and Color Calibration

In medical imaging systems, light quality directly impacts image clarity, color fidelity, and clinical interpretation. Devices such as endoscopes, surgical visualization systems, and diagnostic displays rely on tightly controlled illumination to ensure anatomical features are accurately represented. Even minor spectral shifts or brightness inconsistencies can affect contrast, color rendering, and diagnostic confidence.

Our innovative Features

Light and Color Calibration Technology


Confidence in Clinical Image Accuracy

Spectroradiometric measurement ensures illumination systems produce consistent, repeatable spectral output. This enables medical imaging systems to present anatomy with accurate color representation and contrast, supporting more confident clinical interpretation.

Reliability Across Development and Production

Consistent measurement technology enables engineers to correlate R&D characterization with manufacturing quality control. This continuity ensures devices perform as intended when scaled from prototype to volume production.

Reduced Risk of Imaging Variability

By measuring absolute spectral performance rather than relative light levels, spectroradiometers reveal subtle shifts that can degrade image quality over time. This helps manufacturers identify and correct variability before it affects device performance.

Accurate Measurement in Complex Optical Systems

Medical illumination systems often operate at low intensities and within tightly controlled spectral ranges. Spectroradiometers precisely calibrate these light sources to ensure consistent, accurate illumination that enables correct image rendering on medical displays.

Traceable Verification for Regulated Devices

Spectroradiometers provide traceable, quantitative data that supports verification, validation, and documentation requirements. This allows manufacturers to demonstrate controlled optical performance throughout development, production, and lifecycle testing.

Protection of Long‑Term Imaging Performance

Over time, light sources can drift in brightness and spectral composition. Using a spectroradiometer for light and color measurements allows manufacturers to monitor and maintain illumination performance, supporting long‑term device reliability and consistent visual output.

Robotic Surgery & Endoscopic Imaging Systems

In robotic and endoscopic surgical systems, precise calibration of the light source is critical to ensure accurate color representation of tissue and anatomy during minimally invasive procedures. Spectroradiometers are used to calibrate illumination so images render consistently on surgical displays.

  • Verify spectral output of surgical light sources
  • Detect brightness and color drift
  • Supports repeatable calibration across systems used in development, production, and service

Diagnostic Medical Imaging & Visualization Equipment

Diagnostic imaging systems rely on calibrated illumination to deliver consistent brightness, contrast, and color performance. Spectroradiometers are used to validate and maintain light source performance so images are presented correctly on medical displays.

  • Validate imaging illumination performance
  • Detect spectral and brightness drift over device lifetime
  • Traceable calibration data to support verification and quality control

Dental Imaging & Color Matching Systems

In dental applications, spectroradiometers are used to calibrate light sources and imaging systems for accurate color matching of crowns, bridges, and restorative materials. Precise light and color measurement ensures consistency between imaging, manufacturing, and final appearance.

  • Accurate dental color matching
  • Consistent illumination conditions across imaging and fabrication workflows
  • Shade matching for improved patient outcomes and aesthetics

Surgical Lighting & Clinical Illumination Systems

Surgical and clinical environments require stable, uniform illumination to support accurate visualization during procedures. Spectroradiometers are used to calibrate and validate lighting systems used in operating rooms and clinical settings.

  • Precise spectral measurement of surgical lighting systems
  • Verification of color temperature and luminance consistency
  • Monitoring to maintain illumination quality over time

FAQs

Medical device manufacturers use spectroradiometers instead of simpler light meters because they provide full spectral data, enabling highly accurate color and luminance measurements critical for display calibration and visual diagnostics. This level of precision ensures consistent, true-to-life color performance across medical displays, which basic light meters cannot achieve.

The best spectroradiometer depends on your specific medical application requirements, including measurement range, accuracy, and form factor. Contact our technical team at support@novanta.com or complete the Contact Us form at the bottom of this page to discuss your needs—we’ll help you select the right solution for your application.

Overall, the accuracy of a spectroradiometer is determined by the precision of calibration, the quality of the optics, and the detector’s response characteristics. Many advanced models, such as the Photo Research® 700-Series, spectral measurement resolutions as fine as a few nanometers and can provide measurements with an accuracy of better than ±1% in intensity and ±2% in color coordinates. This level of precision is vital for ensuring consistency in color reproduction and for developing lighting solutions that deliver the desired aesthetic vision in fields such as cinematography.

Spectrometers and spectroradiometers are analytical instruments used to measure properties of light and color. A spectrometer only measures the spectrum of light emitted, absorbed, or scattered by materials by analyzing the specific wavelength of light. In contrast, a spectroradiometer measures the intensity of light and color across a range of wavelengths. This is what makes spectroradiometers particularly desirable in applications that required a high-level of detail about light and color measurement.

Contact Us

This consultative sales style, combined with our family of standard and customizable products, ensures that you always get the best product for your application.

This field is for validation purposes and should be left unchanged.
Full Name(Required)
Address