technical papers

Introducing RFID into Next-Gen Automated In-Vitro Diagnostic Testing to Enhance Workflow Precision and Accuracy

Published on April 2, 2026

Published

Reading time

Category

Medical laboratories are tasked to provide the analytical basis for highly critical medical decisions. “According to official data, 60–70% of clinical decisions about hospitalization, discharge, and prescription are based on laboratory results.”1 In the context of public health, any error rate plays a significant indicator as to the quality of these decisions. However, total quality is an interconnected property in workflows and from initial steps all analytical stages must be under monitoring and quality control. Read more…

Latest Insights & Resources

Explore our most recent blogs, technical papers and articles showcasing real-world use cases and how our technologies help solve critical challenges in medical, industrial, and retail applications

Contact us

This field is for validation purposes and should be left unchanged.
Full Name(Required)
Address
This field is hidden when viewing the form

Please complete this form to download the file

Your download should begin immediately.

This field is for validation purposes and should be left unchanged.
Name(Required)
Address(Required)
This field is hidden when viewing the form